LTE TDD

Cell Parameters Downlink (Basic TDD)

For Waveform Playback (ARB) capability.

This topic describes the settings of the Downlink > Cell Parameters node for a Basic TDD carrier.

State

Total Number of Antennas

Antenna Port

Power Definition Type

Reference Signal Transmit Power (RSTP)

OFDM Symbol Transmit Power (OSTP)

State

Turns the downlink transmission on or off.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:STATe ON|OFF|1|0

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:STATe?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DL:STATe ON

RADio:LTETdd:WAVeform:CCARrier:DL:STATe?

Preset

On

State Saved

Yes

Initial S/W Revision

A.20.01

Total Number of Antennas

Sets the total number of antennas for downlink transmission. Determines which Antenna Port values are available.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:APORts:COUNt AT1|AT2|AT4|AT8

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:APORts:COUNt?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DL:APORts:COUNt AT1

RADio:LTETdd:WAVeform:CCARrier:DL:APORts:COUNt?

Couplings

Drives the available Antenna Port selections.

Preset

AT1

State Saved

Yes

Initial S/W Revision

A.20.01

Antenna Port

Selects the antenna port used for downlink transmission.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:APORt PORT0|PORT1|PORT2|PORT3|PORT4|PORT5|PORT6|PORT7

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:APORt?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DL:APORt PORT0
RADio:LTETdd:WAVeform:CCARrier:DL:APORt?

Couplings

The available port selections are determined by Total Number of Antennas.

Preset

PORT0

State Saved

Yes

Initial S/W Revision

A.20.01

Power Definition Type

Sets the power reference for the downlink.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:POWer:DEFinition TOTal|RSTP

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:POWer:DEFinition?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DL:POWer:DEFinition TOTal

RADio:LTETdd:WAVeform:CCARrier:DL:POWer:DEFinition?

Notes

When TOTal: RSTP and OSTP are read-only.

When RSTP: Total Carrier Power and OSTP are derived.

Dependencies

Controls read/write state of RSTP and drives OSTP.

Preset

TOTal

State Saved

Yes

Initial S/W Revision

A.20.01

Reference Signal Transmit Power (RSTP)

Displays the reference signal transmit power, in dBm.

See 3GPP TS 36.141.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:RSTP?

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:RSTP <rel_ampl>

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DL:RSTP -144

RADio:LTETdd:WAVeform:CCARrier:DL:RSTP?

Dependencies

This setting is editable when Power Definition is set to RSTP otherwise it is read-only.

Couplings

Derived from Power Definition Type, carrier power, and signal settings.

Preset

-40.79 dBm

State Saved

No

Min

-144

Max

-15

Initial S/W Revision

A.20.01

OFDM Symbol Transmit Power (OSTP)

Query only

Displays the OFDM symbol transmit power, in dBm.

See 3GPP TS 36.141.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DL:OSTP?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DL:OSTP?

Couplings

Read-only. Derived from Power Definition Type, carrier power, and signal settings.

Preset

-13.01 dBm

State Saved

No

Initial S/W Revision

A.20.01

Carrier Downlink (Basic TDD)

Welcome to LTE TDD